News Overview

First trade fair hackathon with PLCnext Technology

24.09.2018

First trade fair hackathon with PLCnext Technology

[5071] In 2016, the open control platform based on PLCnext Technology from Phoenix Contact was unveiled at SPS IPC Drives.

The new solution converts a traditional PLC into an open control platforms that can be programmed in IEC 61131, high-level language or model-based code. In addition, the PLCnext Store that Phoenix Contact has now launched on the market is a software store where users can load apps onto the control platform during the code creation process. PROFICLOUD, which is a professional cloud solution, rounds out the automation ecosystem. Thanks to the openness of the complete solution, Phoenix Contact offers numerous options for linking the traditional automation world with the IT world and generating new business models based on software and data. These are ideal conditions for participating in the first automation hackathon at SPS IPC Drives 2018.

Interested parties can sign up for the hackathon at www.elektrotechnik.vogel.de/automation_hackathon/ which will take place at the trade fair grounds of NCC West in Nuremberg on November 25 and 26, 2018. The required infrastructure, special equipment, and catering are provided. In addition, Phoenix Contact PLCnext specialists will provide you support in implementing your ideas. It is up to the participants to select a specific application from the B2B area and the addressed industry. You will then present your solutions to a large audience of professionals in the trade fair forum on November 27, 2018. In addition to cash prizes totaling 15,000 euros, outstanding concepts can be transferred to an app that can be distributed through the PLCnext Store.