News Overview

Tailored specifically to the system

07.10.2019

Preconfigured CBMC device circuit breaker

[5158] The new CBMC ... S-R-C multi-channel electronic circuit breakers from Phoenix Contact can be ordered directly in versions that are tailored specifically to the system.

In addition, the integrated status output and reset input allow the device status to be monitored remotely and tripped channels to be switched on again.

The new versions therefore combine two features in a single device, enabling you to benefit from faster installation and the ability to reset devices remotely, which saves costs during startup and servicing. The device circuit breakers also include established features, such as one-button operation via the LED button and the electronic interlock to prevent unintentional changes to current values.

There is also a version that satisfies the requirements of NEC Class 2. The device circuit breakers are available starting from a minimum quantity of one unit.


PHOENIX CONTACT
GmbH & Co. KG

Corporate Communications
Flachsmarktstr. 8
D-32825 Blomberg
+49 5235 3-41240

More Information