News Overview

New CBMC device circuit breaker versions

28.09.2018

Device circuit breaker with status output and reset input

[5075] The CBMC range of electronic circuit breakers has been extended to include a version with a status output and reset input for greater diagnostic and control options.

The main highlight is that it can be switched on again remotely. Due to this function, the device circuit breakers can also be installed in isolated locations or those that are difficult to access.

Another version electrically interrupts load outputs with the help of built-in relays. This means that in the event of an error the protected output is not just switched with high impedance via a MOSFET, as is the case with the majority of electronic circuit breakers. In some applications electrical isolation is required in the event of an error.