News Overview

Phoenix Contact E-Mobility successfully certified in accordance with IATF 16949

01.02.2018

Lady standing at a charging station, charging an electric vehicle

[5023] Within the Phoenix Contact Group, Phoenix Contact E-Mobility GmbH is the center of expertise for electromobility components and solutions.

Its portfolio includes charging systems and charging controllers for DC and AC charging of electric vehicles. Combined with the right software, it is also possible to implement customized and high-performance charging infrastructure.

For the vehicle-side charging process interface, Phoenix Contact offers what are known as vehicle inlets, which are built directly into the vehicle. Collaborating with automobile manufacturers brings with it particularly stringent demands in regard to work processes, product quality, and organizational structure. Certification in accordance with IATF 16949:2016 was established within the automotive industry to ensure these requirements are being met uniformly and internationally. Quality management system certification in accordance with ISO 9001:2015 is also a substantial component of this standard. Phoenix Contact E-Mobility GmbH recently acquired certification in accordance with both of these standards, and now meets the stringent requirements of the automotive industry.