Punctuation

Hyphen ( - )

To separate the words in a compound adjective, verb, or adverb.

 

When to hyphenate:

Backup/back-up, startup/start-up, runtime/run-time, login/log-in, etc.

UsageExample
Use one word when used as a noun.We provide a reliable power supply backup.
Use hyphen when used as an adjective.We suggest a back-up power supply.
Use two words when used as a verb.Back up your power supply.
Zurück nach oben

Single mode and multimode

UsageExample
When used to describe a product, hyphenateA single-mode terminal block
When used as a noun, use two wordsChoose single mode

Prefixes and suffixes (e.g., multimode)

In general, do not use a hyphen to set off a prefix at the beginning of a word or a suffix at the end of a word.

Therefore, multimode should be used as one word.

Here are a few important exceptions to this rule:

UsageExample
When the prefix ends in “i” or “a” and the following word begins with the same vowel, use the hyphen.
  • Multi-institutional
  • Ultra-active
Hyphenate the word whenever not doing so can lead to misreading.
  • Buy a co-op.
  • Chickens are in the coop.
  • Multiply by 20.
  • Use multi-ply fabric.
  • It is a unionized factory.
  • It is an un-ionized product.

En dash (–)

UsageExample
To express a range of values or a distance12 – 24 inches
Zurück nach oben

Em dash (—)

UsageExample
To separate the final part of a sentence that is logically not part of the sentence.Phoenix Contact offers various types of cables — copper, fiber optic and photovoltaic, among them.
To set off parenthetical elements, which are abrupt.The PC — with a fanless design — increases system availability.
Zurück nach oben

Semicolon ( ; )

UsageExample
To join independent clauses in compound sentences that do not have coordinating conjunctions and commas as connectorsAutomation can be costly and complex; however, with the right control solution, it can become simple and cost-effective.
To separate items in a series that already includes commasPhoenix Contact has offices in the following United States cities: Houston, Texas; Ann Arbor, Michigan; and Middletown, Pennsylvania.
Zurück nach oben

Colon ( : )

UsageExample
After an independent clause that precedes a listPhoenix Contact hand tools offer the following benefits: durability, comfort, interchangeability and reliability.
To separate an explanation, rule or example from a preceding independent clauseWe call it functional safety: reliable protection for people and machinery.
When depicting time, to separate hour and minutesThe typical work day begins at 8:00.
Zurück nach oben

Apostrophe ( ’ )

UsageExample
To indicate ownership by a proper nounThe president’s office is on the first floor.
To indicate ownership by a plural nounThe employees’ vehicles are parked in the parking lot.
Within a contractionDo not becomes: don’t.
To abbreviate a year2012 becomes: ‘12.

DO NOT use an apostrophe when:

  • Indicating ownership using the word “it”
  • Indicating a plural
  • Making an abbreviation or acronym plural

 

Zurück nach oben

Comma ( , )

UsageExample
To separate elements in a seriesCrimping, cutting, electronics, and riveting tools are available.
To connect two independent clausesThe cable was disconnected, thus the system was unable to run.
To separate introductory clausesBecause of the ergonomic handle design, the hand tools allow natural hand posture.
To separate city and state when depicting locationMiddletown, Pennsylvania

Note: A comma should never be used between a subject and its verb.

Zurück nach oben

Exclamation Point ( ! )

  • Within a quotation
  • After interjections, such as “Wow!”
  • To express surprise, astonishment, or any other strong emotion to add additional emphasis

Note: Exclamation points should be used sparingly, particularly in formal writing. In addition, multiple exclamation points following a sentence should be avoided.

Zurück nach oben

Bullets

Do not put a period at the end of bullet points.

  • Only one sentence per bullet
  • If it can’t be combined, add another bullet
Zurück nach oben

PHOENIX CONTACT
GmbH & Co. KG

Flachsmarktstraße 8
D-32825 Blomberg
+49 5235 3-00