electronica 2018

electronica 2018 –
The world's leading trade fair and conference in electronics

Visit Phoenix Contact at the world's leading trade fair for electronics.

November 13 - 16, 2018 in Munich
Hall B3, Booth 103

Welcome to Phoenix Contact at electronica 2018.

We look forward to seeing you again, this time at Booth 103 in Hall B3.

In keeping with our motto “Best connectivity for a smart world”, Phoenix Contact will be presenting future-oriented connection technology at electronica in Munich. Smart electronics solutions demand intelligent and uniform interfaces. Tailor-made PCB connections, connectors and electronics housings are the basis for the intelligent networking of decentral components.

Visit us at the world's leading electronics trade fair and see the exceptional quality of our products for yourself. You will also find tailor-made solutions in our Service World for device manufacturers. These range from configuration through digital networked processes all the way through to customer-specific innovations. Our range is rounded out by marking and installation systems, innovative power supplies, device protection, and the latest charging cables for your electric vehicle.

With creative solutions in the fields of connection technology, electronics, and automation, Phoenix Contact is your key partner on the path to a smart world. With Phoenix Contact by your side, you are ideally prepared for the digital transformation and can become an Industrie 4.0 company.

Be our guest at the electronica

Reserve your free ticket for the electronica trade fair in Munich. Simply complete the form provided below and we will send you a unique voucher code. You can redeem this in the electronica 2018 Ticket Shop.

Our exceptional innovations at the electronica 2018

Phoenix Contact is presenting a variety of different products and solutions at the electronica 2018. We would like to give you a sneak preview of these before the trade fair begins.

PTFIX is the new system for potential distribution solutions in devices tailored to individual requirements. The system consists of connection-ready blocks with Push-in technology in many different colors, numbers of positions, and mounting types. The blocks, with up to 18 terminal points, can be combined in any way and mounted on DIN rails or directly – they can even be glued onto flat surfaces. The configurator provides you with support in selecting the desired combination, including online pricing and a rapid order option.

Easy device connection with the panel feed-throughs of the new IPD pluggable installation system with secure and convenient on-site fast locking system. The Push-in connection enables time-saving assembly. Experience easy device connection with the new IPD pluggable installation system. Install conveniently and securely with the on-site fast locking system. Furthermore, the Push-in connection system enables automatic wiring with wiring robots. The IPD panel feed-throughs are therefore ideal for lighting applications.

Signals, data and power are the essential electrical transmission types in an industrial facility. Compact and powerful M12 connectors are ideally suited for this environment. Established as the industry standard for signal and data applications, they are also increasingly being used for power transmission in devices that are becoming ever more compact. M12 POWER offers maximum performance in a compact design.

With PROJECT complete, you can configure your terminal strip and then easily create the associated markings. The software provides ideal support throughout the process and automates many tasks. Experience the perfect digital networking of all process steps, from CAE configuration through to the assembly of the finished product.

Create marking solutions more easily than ever before with the Phoenix Contact MARKING system. The THERMOMARK ROLLMASTER roll printer is particularly well suited to marking electronic components. It processes large volumes of material very rapidly. The new BLUEMARK ID printing system provides maximum flexibility: using environmentally sound UV LED technology, it marks more than 1,350 different marking materials – even in color.

Powerful, SIL3-certified QUINT POWER power supply – also for the Ex area. The new QUINT DC UPS with integrated interface for PROFINET, EtherNet/IP, EtherCAT, or USB for your existing network.

A complete range of electronic device circuit breakers for your power supply system. Perfect control of your system statuses with single and multi-channel products.

Experience High Power Charging (HPC) live at the electronica. With this new technology, you can charge your electric vehicle for a range of 100 km in just three to five minutes. This is made possible by an intelligent cooling system, which allows charging stations to reach charging powers of up to 500,000 watts.

Convince yourself at electronica of the excellent design of our new AC charging cables, which recently received the German Design Award 2019. The charging cables convinced the jury with their functionally well solved design, the comfortable feel and the modern design language.

Review of electronica 2016

electronica 2016 drew 74,000 visitors and more than 2,900 exhibitors from 51 countries.

Phoenix Contact is pleased that the 2016 trade fair was such a success. A statement by the president of the Device Connectors division, Torsten Janwlecke:

As the meeting place for the electronics industry, electronica is and remains one of the most important international platforms for Phoenix Contact. At electronica, we encounter many users with specific technical requirements. The ensuing discussions were highly productive for both sides. We were delighted that our intelligent devices and solutions attracted so much interest. It's the combination of performance and technical depth what makes electronica so special for me. This is where promises are not only made, they are also kept.

More interesting observations and statements can be found at the electronica 2018 website.

Our tips for your visit to electronica

You can find directions to the trade fair in Munich here.

Whether by car, train, plane, or public transportation – the Munich trade fair site offers an outstanding traffic infrastructure. Traveling by subway? Use line U2 which runs every 5 minutes. The subway stops at both Messestadt West and Messestadt Ost can be reached in 18 minutes from the city center.

The traffic routing system at the trade fair site will guide you to free parking spaces. The site features several parking areas in the open, as well as the multistorey car park 'Parkhaus West'. Parking fees are 10 or 12 euros per day.

During the trade fair, demand for hotels near the trade fair site is very high. Feel free to look for something a bit further away. The city of Munich and its immediate surroundings offer excellent accommodation.

electronica 2018 trade fair information

We look forward to seeing you again at the Phoenix Contact booth at the world's leading trade fair for components, systems, and applications in Munich:

  • November 13 - 16, 2018
AddressOpening times

Messe München GmbH
Messegelände
81823 München, Germany

Daily from 9:00 a.m. to 6:00 p.m.
Fridays from 9:00 a.m. to 5:00 p.m.

Held in Munich every two years, electronica is the world’s leading trade fair for components, systems, and applications in electronics, and is being held again in 2018. Technologies, products, and solutions from the electronics sector right across the board will be presented at the trade fair. This year's electronica showcases current developments in the electronics industry and rounds this off with an insight into trends.

This year, the number of attendees and exhibitors to electronica will once again exceed those of previous years and will, for the first time, be accompanied by the SEMICON Europa event. With more than 450 exhibitors, it is Europe's leading trade fair for industry and research in the areas of flexible hybrid electronics, smart production, power electronics as well as medical engineering.

In addition, the world's leading trade fair in electronics will be accompanied by further regional leading trade fairs in India, Asia, and China, which also focus on the areas of electrical manufacturing as well as applications, systems and components of electronics.

The trade fair in Munich offers a series of theme-oriented forums as well as five conferences which cover topics such as Automotive and Wireless. For further information, please refer to the relevant web page of electronica 2018:

More about the forums and conferences of electronica 2018

PHOENIX CONTACT
GmbH & Co. KG

Flachsmarktstraße 8
32825 Blomberg, Germany
+49 5235 3-00

See more oft he electronica on YouTube

Experience our exhibition highlights on our YouTube channel.

Phoenix Contact YouTube Channel
To the YouTube channel

Our booth

Download a map of our both and use it for your visit at the fair.

Our booth
Open map [PDF, 27 KB]
Referrer: https://www.phoenixcontact.com/online/portal/pc

This website uses cookies, by continuing to browse, you agree to our cookie policy. Read our privacy policy for more information.

Close