News Overview

NearFi couplers for contactless power and data transmission

04.05.2021

NearFi couplers transmit power and data across an air gap

[5335] With the launch of NearFi, Phoenix Contact is introducing a new, innovative technology for contactless power and data transmission in the near-field range to the market. This is the first technology to enable wireless, protocol-independent and latency-free Ethernet communication at speeds of up to 100 Mbps across an air gap of up to 10 mm.

One of the first applications of this technology is in the new NearFi couplers, which will replace wear-prone connectors or slip rings in industrial applications. This is especially helpful in situations where these parts are reaching their limits due to contamination, vibration, or frequent contact.

The couplers can be mounted easily and flexibly with the universal mounting options. They can be brought together from any direction or in rotation and do not have to be positioned exactly on top of each other. The all-around visual signaling with bright LEDs displays the operational readiness of the coupling link in all spatial directions. With robust IP65 housings with M12 connections for Ethernet and power, the NearFi couplers can also be used in demanding environments.


PHOENIX CONTACT
GmbH & Co. KG

Corporate Communications
Flachsmarktstr. 8
D-32825 Blomberg
+49 5235 3-41240

More Information