News Overview

Expansion modules for PLCnext Control controllers

01.04.2019

Left-alignable Ethernet interface  

Left-alignable Ethernet interface

From now on, users can operate even more individual requirements with the PLCnext Control controllers from the Axiocontrol series from Phoenix Contact: The interfaces of the PLCnext Control can be adjusted using expansion modules.

These expansion modules are then connected to the left side of the controller and operated. The first module provides an extra Ethernet interface with an additional MAC address. Configuration is performed via the PLCnext Engineer software.

In the future, additional bus-specific modules for INTERBUS and PROFIBUS will be added to this Ethernet expansion module. Both variants will include a master function to connect existing INTERBUS and PROFIBUS participants.


PHOENIX CONTACT Ltd

Unit 15C, 906-930 Great South Road, Penrose
Auckland 1061
New Zealand

Phone: 0508 474 636
Toll Free (Local)
09 950 8495

More Information

This website uses cookies, by continuing to browse, you agree to our cookie policy. Read our privacy policy for more information.

Close