News Overview

Bluetooth adapter for data exchange with mobile terminal devices

23.11.2015

Bluetooth adapter  

Convenient data exchange with new Bluetooth adapter

The new Bluetooth adapter from Phoenix Contact enables data exchange between Interface products and mobile terminal devices.

Wireless connections therefore enable more convenient control and regulation processes in industrial applications. The adapter is available as an accessory for MINI Analog Pro, MINI Analog, PLC logic, and Interface System Gateways products. Depending on the device type, it is either connected via the µUSB or S-PORT interface. If a PC or laptop is used for configuration, the accompanying PC adapter should also be used to ensure error-free communication. It is connected to a free USB connection on the PC. A corresponding driver is included in the software solutions of the devices to be programmed.


PHOENIX CONTACT Ltd

Unit 15C, 906-930 Great South Road, Penrose
Auckland 1061
New Zealand

Phone: 0508 474 636
Toll Free (Local)
09 950 8495

This website uses cookies, by continuing to browse, you agree to our cookie policy. Read our privacy policy for more information.

Close