News Overview

DC charging controller for modern fast charging stations

01.03.2019

EV Charge Control Professional DC charging controller  

The EVCC Professional DC charging controller is the solution for modern fast charging stations

EV Charge Control Professional is our high-performance controller solution for fast charging stations in the public and industrial sector, such as electric charging stations along freeways.

You can operate two independent charging points with the controller: one for fast DC charging in accordance with DIN SPEC 70121 and another for conventional AC charging as per IEC 61851-1. It takes care of all control and communication tasks within the charging station, including visualization on the operator panel. You can also implement a CHAdeMO interface using software modules.

Ethernet, RS-232, RS-485, and CAN-bus interfaces are used to flexibly combine all of the necessary charging station components in an overall system. The charging station can then be integrated into your charging park, building or energy management system. The programmable PT1000 input ensures that the controller can continuously monitor the temperature at the power contacts of the vehicle connector. Depending on the programming, the charging process can either be switched off or the charging power can be reduced in the event of overheating. The integrated 3G mobile network modem also facilitates easy remote access. The pluggable Push-in connection terminal blocks ensure the controller can be installed quickly without tools.

The controller can be freely and individually programmed using the PC Worx software in accordance with international standard IEC 61131. The 16 digital inputs and outputs can be used flexibly during this process. The controller is thus very versatile and can be used for various requirements and system architectures. During programming, you can reduce the engineering work by using ready-made function blocks for vehicle communication that can display complete charging processes. The license for these blocks is provided separately on an SD card that you can also use as a programming and configuration memory in the charging controller.