News Overview

Y-distributor separates CAT5 and power

11.07.2016

Y-coded Y-distributor  

Easy integration of devices with Y-coded M12 interface

A Y-coded interface transmits both data and power while also reducing the number of cables in the system.

The new Y-coded Y-distributor from Phoenix Contact enables you to easily integrate devices with hybrid M12 interfaces. It has a Y-coded interface on one side and an A and D-coded interface on the other side. It therefore satisfies CAT5 requirements. This means that you can also integrate new sensors in existing cabling. A and D-coded standard cables that are already in use can be retained. The SPEEDCON fast locking system reduces assembly time.


PHOENIX CONTACT Ltd

Unit 15C, 906-930 Great South Road, Penrose
Auckland 1061
New Zealand

Phone: 0508 474 636
Toll Free (Local)
09 950 8495

More Information