News Overview

Valueline IPC wins a reddot design award

2015/03/30

The new generation of Valueline industrial PCs combines perfectly functional design and high-performance technology, which won over the jury of the red dot design award.

Among 5,000 submissions from 56 countries, Valueline IPC is one of the best in its class. It was awarded the Product Design category of the prestigious reddot Design Award 2015.
Industrial PCs with touch display, so-called panel PCs, are increasingly becoming the central interface between humans and machines. The HMI  (Human Machine Interface) combines all the operating and monitoring processes, as controls, buttons, and sliders can now be found on the  display. At the same time, a high-performance computer is used for all the control and visualization tasks in the system. Thus, a combination of state-of-the-art computer technology and user-friendly design is all the more important.