News Overview

Managed Switches for growing networks

2018/04/20

New Managed Switches from the FL SWITCH 2000 product range  

Perfectly suited for the design of growing networks: The new 16-port switches from the FL SWITCH 2000 series

The new versions of the 2000 Managed Switches enable the connection of up to 16 network devices

With the new 16-port versions, Phoenix Contact is extending its range of Managed Switches in the FL Switch 2000 product range to accommodate the increasing number of Ethernet-capable devices in automation networks.

The flexibility of the wide range of connections with up to four fiberglass ports, combo ports and various FO connection methods in the SC, ST/BFOC, and LC classes will continue to be available in the new versions. In addition, the user can select the appropriate range of functions as well as Gigabit versions for high communication requirements for his application from the extended portfolio.

Furthermore, with the new power supply connector with Push-in Technology, device installation is much faster. Thanks to the consistent front operation, automated cabling is also possible.