News Overview

A new version of the Waterworx library is available

2015/09/11

Waterworx software box  

Efficient engineering for Water and Wastewater Treatment

The new version of the Waterworx function block library from Phoenix Contact now offers even more engineering possibilities in the Water and Wastewater Treatment sector.

An open OPC interface in the blocks facilitates connection to standard control systems. Multi-vendor field devices can also be integrated via a Modbus, PROFINET, or PROFIBUS interface. Function blocks have also been optimized with integrated diagnostic functions. The library is now supplied in the new version via a pluggable program and configuration memory. This can be enabled using the valid license key on the controller. Without a valid license, blocks can be tested in demo mode for a limited period of time.