News Overview

New generation of TP 5000 touch panels

2015/12/14

TP 5000 touch panels  

Touch panels with high-performance PC platform

The TP 5000 series touch panels are being converted to a new hardware platform.

The change has become necessary because the current hardware platform has been discontinued. With a smooth transition in mind, we have converted to the recess-compatible hardware of the Basicline panel PC. There are still three different display sizes: 12.1 inch (30.73 cm), 15 inch (38.1 cm), and 17 inch (43.2 cm) available.