News Overview

Active PROFIBUS termination resistor

2016/07/11

Active PROFIBUS termination resistor  

The active termination resistor allows the termination of PROFIBUS networks

The termination of PROFIBUS networks is now performed by the new active PSI-TERMINATOR-PB-TBUS termination resistor.

This device relies on permanent termination to ensure interference-free communication, particularly in applications that involve alternating bus devices. The bus line can be connected either via a plug-in double spring terminal block or a D-SUB socket. Alternatively, the active programming and diagnostic devices can be supplied with voltage using the D-SUB connection. This also makes the device suitable for use as a defined service and measuring-device connection within a bus system. LED displays with bus activity and the redundant power supply are available to the user for local diagnostics.