News Overview

Phoenix Contact E-Mobility expanding to Poland

2020/07/08

Electric motorbike charging at an HPC charging station  

Phoenix Contact provides almost all of the components needed for modern and powerful charging stations

We are expanding our production capacity with a new facility in Poland. The 15,000 m² plant at the Science and Technology Park Rzeszów-Dworzysko will be built by full-service logistics and commercial real estate developer Panattoni. The new facility is set to be completed by the end of 2020/start of 2021.

Among other things, we will use the new production location for the manufacture and testing of various AC and DC charging cables that are supplied to leading automobile and charging infrastructure manufacturers. The new building provides a total area of 15,000 m², which is divided into 14,000 m² of production and storage space and 1000 m² of office space. Production is scheduled to commence at the start of 2021 and the workforce will increase to over 250 employees within the next few years. In addition to his role as Sales Director at our headquarters in Schieder-Schwalenberg, Marwin Achenbach will also head up the management team responsible for our new facility.

Rzeszów will be an important location in our global production network. It will play a particularly significant role in international collaboration between locations in Germany, Poland, and China. In addition, IATF-compliant production and business processes will be implemented to ensure that our innovative products meet high quality requirements. Project manager Christoph Paetzold purposefully chose the dynamic and fast-growing university city of Rzeszów because it is situated close to an airport and benefits from a well-developed road infrastructure, which offers many advantages from a logistics point of view. There are already many well-established companies located in the area, including aerospace companies, which is why the region is also known as Aviation Valley.


Phoenix Contact UAB

Svitrigailos str. 11B
03228 Vilnius
+370 5 210 6321