Solutions for power station markings

Application

Power station  

Power station

The power station marking system (KKS) is a marking system for the uniform and systematic marking of power stations. The Reference Designation System for Power Plants (RDS-PP) is a modern replacement for the proven power station marking system. It provides a number of innovations and additions that accommodate modern requirements for the marking of power station components.

In contrast to KKS, RDS-PP has been developed further with the focus also on new forms of power generation, such as distributed systems, and is used by all specialist units for planning, approval, installation, operation, and maintenance. The marking in accordance with KKS and RDS-PP consists of a 15 to 17-character alphanumeric designation. The letters are usually used to classify the systems and units. The numbers are used for counting.

Identification types

Identification types

To meet increasing pressure on costs, streamlined and efficient maintenance processes are essential for on-site testing and maintenance work on the unit and equipment. Here, the traditional method of creating job orders and test reports in hardcopy form can be replaced cost-effectively first and foremost by modern identification and communication systems that are suitable for industrial applications. Furthermore, information can be exchanged using the central documentation and maintenance system, obviating any need for paper. It is above all the identification method, such as bar code, QR code or RFID, that plays an increasingly important role here. Mobile and electronic maintenance processes can therefore be designed in an optimum and paperless way.

Identification via bar code

Bar code with Phoenix Contact founding year

Bar code

Bar codes are already frequently used for forward-looking, mobile maintenance in station identification. However, due to the stringent demands of the environment, bar codes have proven a less than ideal solution for labels, especially in a power station. Dirt and aging often lead to high error rates and limited identification.

Identification via matrix code

QR code

QR code

We support various matrix codes such as QR codes. The matrix code can be used to reliably document relevant information using mobile devices.

Identification via RFID

RFID

RFID UHF

When it comes to RFID technology, a distinction is made between active and passive transponders (transmit and response). The fundamental design of an RFID transponder consists of an antenna, a microcontroller, and a permanent memory that can be read and written. In order to ensure optimized maintenance, passive transponders that do not have a separate battery supply tend to be used in power stations. In the case of passive transponders, a distinction is made between high frequency (HF) and ultra high frequency (UHF) transponders. The HF transponder is excited at a frequency of 13.56 MHz, e.g. using a handheld device. It reaches a maximum distance of 1 m. The UHF transponder, which has a frequency of 868 MHz (central Europe), is suitable for larger distances of up to 4 m. Both transponder types are used in power station applications:

  • Since for electrical equipment, clear identification is the primary aim, greater distances and the associated bulk detection are not possible here. In the case of bulk detection, all RFID transponders within range of the handheld device are detected.
  • In the case of mechanical structures and large units, it is more practical to use UHF transponders due to the inaccessibility of some areas. Bulk detection of multiple RFID transponders is certainly a possibility here.

Pipeline marking

Label carrier with color add-on modules and marking label  

Label carrier with color add-on modules and marking label

As per DIN 2403 guideline requirements, pipelines must be identified according to the medium conveyed using different colors. In addition to pipeline tapes, which do not identify buried pipes at possible danger points, the pipes associated with a unit are usually marked in accordance with the KKS marking system. The colors can be individually assigned by the modular identification system. A carrier is used which can hold a label size of 90 x 38 mm. The label is held in the carrier by the two medium colors that are attached externally and secured by two pop rivets. This allows the label to be swapped quickly if the encryption is changed, without having to remove the carrier.

Solution

Phoenix Contact offers a marking system that enables the flexible implementation of all marking tasks in the power station using a single printer.

The BLUEMARK ID printers

The marking system with marking materials  

The marking system with marking materials

The BLUEMARK ID high-speed printers are at the heart of this marking system. Markings created using the special UV LED printing process meet all requirements associated with a power station environment.

They are resistant to high thermal, chemical and mechanical loads. Thanks to the wide range of marking materials and system accessories, practically all the different marking tasks associated with power station identification are covered.

Your advantages

  • One complete solution – from printing to electronic identification
  • Three identification methods (bar code, QR code, RFID) – one printing system
  • Efficient and paperless documentation and maintenance management
  • Conforms to international standards: ISO, IEC, and VGB (B105)
  • Ensures wipe-proof and scratch-proof marking with environmentally-friendly UV printing technology
  • Additional materials for practically all applications in the power station (conductor, cable, and equipment marking, pipeline and unit identification, media and warning labels)

PHOENIX CONTACT (I) Pvt. Ltd.

A-58/2, Okhla Industrial Area, Phase - II,
New Delhi-110 020
+91.11.30262800