News Overview

Surge protection for SHDSL-applications

04.04.2014

Surge protection adapter for SHDSL interfaces  

Surge protection DT-TELE SHDSL

As a manufacturer of surge protection devices, Phoenix Contact has now launched a protection device for SHDSL systems designed to meet the special requirements of SHDSL data transmission.

The protection device guarantees maximum data security with minimum signal attenuation. The surge protector takes the form of an adapter that can be easily installed between incoming telecommunications cables and a modem. The pluggable connection ensures fast, flexible installation. The protection device only needs to be grounded by way of the black cable or DIN rail base. The device features a sturdy metal housing with space for two SHDSL ports.


PHOENIX CONTACT (I) Pvt. Ltd.

A-58/2, Okhla Industrial Area, Phase - II,
New Delhi-110 020
+91.11.30262800