News Overview

Valueline panel PCs win German Design Award

27.03.2017

Valueline panel PC next to the German Design Award logo  

Winner of the German Design Award

The new generation of Valueline panel PCs from Phoenix Contact have received the renowned German Design Award 2017.

The panel PC series impressed the international jury with its attractive design and powerful technology. The panel PCs can be used to reliably implement all operating and monitoring processes in the system. The devices feature a multi-touch screen and are suitable for installation in the front of the control cabinet, which is why the combination of state-of-the-art computer technology and an attractive design is all the more significant. The user can choose between different performance classes and display sizes ranging from 7.0 to 21.5 inches. The industrial PCs have a fanless design and have no moving parts, making the devices failsafe and durable.


PHOENIX CONTACT (I) Pvt. Ltd.

A-58/2, Okhla Industrial Area, Phase - II,
New Delhi-110 020
+91.11.30262800

More Information