News Overview

Hybrid motor starters for I/O-Link

13.11.2017

CONTACTRON hybrid motor starters with IO-Link interface  

CONTACTRON hybrid motor starters with IO-Link interface

Switch and reverse motors quickly and reliably with the CONTACTRON hybrid motor starters.

The new network-capable versions with I/O-Link interface enable consistent communication between the field and control levels, so that process data such as diagnostic messages or motor current can be easily transmitted.


PHOENIX CONTACT (I) Pvt. Ltd.

A-58/2, Okhla Industrial Area, Phase - II,
New Delhi-110 020
+91.11.30262800