News Overview

Surge protection re-engineered – powerful and protective

06.04.2015

Surge protection with Safe Energy Control technology  

Extremely powerful and durable: surge protection with SEC technology

Lightning and surge protection for the power supply is now extremely powerful and durable. This is made possible thanks to the new Safe Energy Control (SEC) technology with impact-free spark gap from Phoenix Contact.

All the protective devices in the new product range have been completely re-engineered and are based on SEC technology. At the heart of the type 1 lightning arrester is a spark gap that safely prevents line follow currents. In previous protective devices, discharge often caused system fuses to blow, however this is now a thing of the past thanks to the SEC technology. The devices are extremely durable and operate quietly in the background helping to protect the system. The type 2 and type 3 surge protective devices are also designed for high performance and functional safety. Installation, handling, and maintenance are simplified in particular by the compact design and consistent plug-in capability of the arresters.


PHOENIX CONTACT (I) Pvt. Ltd.

A-58/2, Okhla Industrial Area, Phase - II,
New Delhi-110 020
+91.11.30262800