SFB technology

Selective protection

Selective protection

Power supplies with SFB technology provide selective and cost-effective protection for your systems.

For maximum system availability, standard circuit breakers must be tripped magnetically as this is the only way to switch off faulty current paths selectively and ensure that important system parts continue operating without any interruption. With SFB technology, the power supply and DC/DC converter supply several times the nominal current for a short period, thereby providing the necessary power reserve.

Your objective: maximum system availability

Faults can never be avoided completely in production. This means, for example, that short circuits in the wiring or load malfunctions may occur. Nevertheless, machines or systems located in unaffected areas should still continue operating without interruption, insofar as the overall process permits this.

The solution is to provide separate protection for the individual termination devices or smaller function groups. This prevents the unnecessary switch off of unaffected system parts in the event of an error.

Power supplies and DC/DC converters with SFB technology protect your production. SFB stands for selective fuse breaking. In the event of an error, the devices supply six times the nominal current for 12 ms in order to switch off the affected circuit.

Back to top

Cost-effective protection with circuit breakers

Important system parts remain in operation  

SFB technology

Usually additional loads, such as sensors or actuators, are connected to a power supply unit parallel to the controller. In order to minimize downtimes, each of these current paths should be protected individually.

Therefore, if a short circuit occurs, only the faulty path of the power supply will be disconnected and the other loads will continue operating without interruption.

At present standard circuit breakers represent the most cost-effective solution for protecting a circuit. They can be tripped electromagnetically or thermally via a bimetal.

To ensure that they trip within a few milliseconds, the current for the integrated solenoid must always be significantly higher than the nominal current of the circuit breaker.

Back to top

Circuit breaker characteristics

Device circuit breaker with 6 A nominal current  

Magnetic tripping from 30 A

The short-circuit currents required for electromagnetic tripping are usually specified for alternating current (AC) by manufacturers. Users must therefore make sure that the DC values are 1.2 times higher.

Circuit breakers are available with various tripping characteristics; characteristic B or C circuit breakers are mostly used in industrial applications.

For characteristic B, the following currents are required in order to trip the circuit breaker:

  • AC applications: three to five times the nominal current
  • DC applications: three to six times the nominal current

Therefore, under the most unfavorable conditions, 150 A is required to trip a 25 A characteristic B circuit breaker within a few milliseconds.

For characteristic C circuit breakers, the following currents are required:

  • AC applications: five to ten times the nominal current
  • DC applications: five to twelve times the nominal current
Back to top

SFB technology prevents voltage dips

Magnetic tripping within 3 to 5 ms  

Dynamic power reserve

In the event of an error, long cable paths limit the required tripping current. This can delay or even prevent circuit breakers being tripped.

If power supplies provide a lower power reserve, this means that thermal tripping may take several seconds or minutes.

In this case troubleshooting is very easy as you can see which circuit breaker has been tripped. However, during this time the 24 V DC voltage of the power supply has already been interrupted and the controller has failed.

In the worst-case scenario, the current supplied by the power supply unit is so low or it just supplies a brief power reserve of a few seconds meaning that the fuse is not even tripped. As a result troubleshooting is extremely time-consuming and expensive.

With SFB technology, the devices in the QUINT series therefore supply up to six times the nominal current. The circuit breakers are tripped magnetically with this pulse.

Back to top

Cable length and conductor cross section

Distance I is crucial for tripping the circuit breaker  

Observe maximum cable lengths

Whether or not a circuit breaker is tripped fast enough also depends on the length and cross section of the cable via which a load is connected.

It is not just the amount of current that the power supply unit can supply which is crucial here. It is only if the impedance of the faulty current path is low enough that high current can also flow in the short circuit and trip the circuit breaker magnetically.

To determine which power supply is suitable for your application depending on the cable length and cross section, please refer to our configuration matrix.

Back to top

Example of use

Uninterrupted operation of the controller in the event of a short circuit at a load  

Uninterrupted operation of the controller in the event of a short circuit at a load

Example scenario:

  • A power supply (24 V/20 A) supplies a controller and three other loads.
  • Each current path is protected by a circuit breaker (6 A/B characteristic).
  • The current paths consist of 25 m long copper cables (2.5 mm² cross section).

In the event of a short circuit in this example, the 20 A power supply unit supplies six times the nominal current for a short period using SFB technology, i.e., a maximum of 120 A. The circuit breaker is always tripped within 3 to 5 ms with ten times the rated current in the magnetic range of its characteristic curve.

The other loads continue operating, the controller is consistently supplied with 24 V DC and continues running without interruption in spite of the short circuit.

Back to top

In practice

The test shown in this video again illustrates the advantages provided by SFB technology.

Back to top

Device circuit breakers from Phoenix Contact

Thermomagnetic circuit breaker with SFB characteristic curve  

Thermomagnetic circuit breaker

Phoenix Contact's range of thermomagnetic circuit breakers is the first to use the SFB characteristic curve.

This tripping characteristic has been specially developed for use with power supplies that operate on the basis of SFB technology. Combining these two devices ensures particularly reliable tripping in the event of an error, even in the case of long cables between the power supply and termination device.

The SFB characteristic curve is based on characteristic C but its tolerance has been narrowed considerably. The circuit breaker therefore reaches its tripping current faster and so is tripped sooner. This limits the short circuit current and reduces the load on cables and connected devices.

Back to top

PHOENIX CONTACT (Israel) Ltd.

P.O.B. 1799 Industrial Park Hasharon
Quadima 60920
+972-9-8915700

Service


Device circuit breakers

Learning module on how device circuit breakers work.