News Overview

Work safely on photovoltaic systems

18.04.2016

Intelligent photovoltaic panel shutdown SOLARCHECK RSD  

Work safely on photovoltaic systems with SOLARCHECK RSD

The new intelligent SOLARCHECK RSD photovoltaic panel shutdown from Phoenix Contact independently puts photovoltaic rooftop systems into a safe state.

Personnel are protected from electric shock during installation and maintenance or in dangerous situations. Photovoltaic rooftop systems generate DC voltages of up to 1000 volts and cannot be disconnected easily on the DC side. This becomes extremely dangerous if the system is damaged and personnel are working inside. The panel shutdown analyzes the current and voltage conditions on the DC side of the system. Deviations from the normal state or shutdown of the inverter result in automatic shutdown of the photovoltaic panels. The system is restarted automatically when a technically safe environment is present. This Auto Rapid Shutdown technology, developed and patented by Phoenix Contact, is more reliable and faster than any human assessment or manual intervention.


PHOENIX CONTACT (Israel) Ltd.

P.O.B. 1799 Industrial Park Hasharon
Quadima 60920
+972-9-8915700