News Overview

Pre-assembled for the highest demands

25.01.2017

19 splice boxes for OM2 and OM4 fibers  

Ready to splice immediately: pre-assembled 19" splice boxes for OM2 and OM4 fibers

Phoenix Contact now offers new 19" splice boxes for FO-based data cabling of control cabinets or computer centers.

The splice boxes for fiber classes OM2 and OM4 feature a compartment that can be pulled out at the front with 12 or 24 LC duplex connections. The FO pigtails fed into the splice cassettes each have unique color coding to simplify assignment to the front connections. Individual test reports establish the insertion and return loss of each pigtail, so that the pre-assembled boxes made from robust sheet steel are ready to splice immediately.


PHOENIX CONTACT (Israel) Ltd.

P.O.B. 1799 Industrial Park Hasharon
Quadima 60920
+972-9-8915700