Choose the desired topic from the following list, then click on a module, and off you go. Have fun and best of luck!
Comprehensive and clear explanation of the LM-S lightning current measuring system: structure, function, and main features, mains connection, and data evaluation. You will also find out about its advantages.
Start learning module
This tutorial will show you how to start up the LM-S lightning monitoring system easily, by installing the components and making all required settings via the web interface.
Start tutorial
In this tutorial, you will find out how to mount PACT current transformers quickly and safely on power rails. The current transformers convert currents from 1 to 4000 A into secondary rated currents of 1 or 5 A – this even includes safe isolation according to EN 50178.
Start tutorial
SOLARCHECK - the DC monitoring system provides you with reliable information regarding the performance of your photovoltaic system. You can therefore detect errors and take appropriate countermeasures.
Start video
PV Monitor is a web-based visualization based on industrial components and is therefore robust and durable, and supports modular expansion. In the event of an error, system operators are informed immediately via an integrated alarm function.
Start video
"$pageName" on