News Overview

Device circuit breakers now with CSA approval

05.03.2015

CB TM thermomagnetic device circuit breakers  

The thermomagnetic device circuit breakers can now also be used in Canada.

As of February 2015, the thermomagnetic device circuit breakers in the CB TM range feature the CSA test mark and can therefore also be used in Canada.

The circuit breakers feature a consistent plug-in design and provide ideal selective protection against the effects of overload and short-circuit currents.


PHOENIX CONTACT (Ireland) Ltd

C6 The Exchange
Calmount Park
Ballymount
Dublin 12
D12 XE18
Ireland
(01)2051-300