News Overview

Current indicator lever-type disconnect terminal block with Push-in connection

27.06.2018

Clearly identify malfunctions and line breaks in the operating state.  

Current indicator lever-type disconnect terminal block with Push-in connection

Clearly identify malfunctions and line breaks in the operating state using the new PT 4-HE-ILA 100 current indicator terminal with Push-in connection.

The voltage drop is evaluated at a Zener diode in reverse direction and is indicated by an LED. Disconnect the circuit safely using the disconnect lever.

The compact design of the terminal block saves space in the control cabinet. It is identical in shape and bridgeable to standard terminal blocks. You have a comfortable testing option at your fingertips via a test point accessible from both sides. The marking of all the terminal points and the disconnect lever give you a clear view of the arrangement.


PHOENIX CONTACT (Ireland) Ltd

C6 The Exchange
Calmount Park
Ballymount
Dublin 12
D12 XE18
Ireland
(01)2051-300