A Y-coded interface transmits both data and power while also reducing the number of cables in the system.
The new Y-coded Y-distributor from Phoenix Contact enables you to easily integrate devices with hybrid M12 interfaces. It has a Y-coded interface on one side and an A and D-coded interface on the other side. It therefore satisfies CAT5 requirements. This means that you can also integrate new sensors in existing cabling. A and D-coded standard cables that are already in use can be retained. The SPEEDCON fast locking system reduces assembly time.
"$pageName" on