Lightning and surge protection for the power supply is now extremely powerful and durable. This is made possible thanks to the new Safe Energy Control (SEC) technology with impact-free spark gap from Phoenix Contact.
All the protective devices in the new product range have been completely re-engineered and are based on SEC technology. At the heart of the type 1 lightning arrester is a spark gap that safely prevents line follow currents. In previous protective devices, discharge often caused system fuses to blow, however this is now a thing of the past thanks to the SEC technology. The devices are extremely durable and operate quietly in the background helping to protect the system. The type 2 and type 3 surge protective devices are also designed for high performance and functional safety. Installation, handling, and maintenance are simplified in particular by the compact design and consistent plug-in capability of the arresters.
"$pageName" on