You can order the new CBMC ... S-R-C multi-channel electronic circuit breakers in versions that are tailored specifically to your system.
In addition, the integrated status output and reset input allow the device status to be monitored remotely and tripped channels to be switched on again. The new versions therefore combine two features in a single device, enabling you to benefit from faster installation and the ability to reset devices remotely. This saves costs during startup and servicing.
You will also benefit from established features such as one-button operation via the LED button and the electronic interlock to prevent unintentional changes to current values. These features are of course also included in the new products.
There is also a version that satisfies the requirements of NEC Class 2. The device circuit breakers are available starting from a minimum quantity of one unit.
"$pageName" on