News Overview

Research project FastCharge: ultra-fast charging technology ready for the electrically powered vehicles of the future

14.12.2018

Research project FastCharge  

The companies involved presented the latest advances in the field of rapid charging technology

Increase in charging capacity to as much as 450 kW – industry consortium develops technology to make charging electric vehicles as fast and convenient as fuelling with petrol.

The industrial companies involved in the research project FastCharge yesterday presented the latest advancements in the field of fast and convenient energy supply for electrically powered vehicles. The prototype of a charging station with a capacity of up to 450 kW was inaugurated in Jettingen-Scheppach, Bavaria. At this ultra-fast charging station, electrically powered research vehicles created as part of the project are able to demonstrate charging times of less than three minutes for the first 100 kilometres of range or 15 minutes for a full charge (10-80 % State of Charge (SOC)).

The new charging station can be used free of charge right away and is suitable for electric models of all brands with the Type 2 version of the internationally widespread Combined Charging System (CCS), as is commonly used in Europe. In order to meet the demands of fast charging at high capacity, cooled HPC (High Power Charging) cables made by Phoenix Contact are used, which are fully CCS-compatible.

The research project FastCharge is being run by an industry consortium under the leadership of the BMW Group; its other members are Allego GmbH, Phoenix Contact E-Mobility GmbH, Dr. Ing. h. c. F. Porsche AG and Siemens AG. FastCharge is receiving total funding of EUR 7.8 million from the Federal Ministry of Transport and Digital Infrastructure. The implementation of the funding directives is being coordinated by NOW GmbH (National Organisation Hydrogen and Fuel Cell Technology).


PHOENIX CONTACT (Ireland) Ltd

C6 The Exchange
Calmount Park
Ballymount
Dublin 12
D12 XE18
Ireland
(01)2051-300