Back to overview

Cultural monument

Hermann monument  

LM-S on the Hermann monument in Detmold, Germany

This application example shows how the lightning detection system is used on the Hermann monument in Detmold, Germany. The copper statue stands upon a sand-lime brick base. Three grounding cables are connected to the plinth of the statue. This means that if the structure, which is over 53 meters tall in total, is hit by a lightning strike, the lightning surge currents are diverted to ground. The sensors are mounted on these down conductors. The evaluation unit is installed in a control cabinet inside the base.

In the case of this application, early detection of potential damage to the system is not the key objective. However, due to the exposed location and the height of the structure, significant lightning strikes should be expected. The detection of these strikes is used to statistically evaluate lightning strikes and their strength. Such applications are of particular interest for lightning research.

Schematic diagram of a LM-S application using the example of a cultural monument

Schematic diagram of a LM-S application using the example of a cultural monument

PHOENIX CONTACT Ltd

Halesfield 13
Telford
Shropshire
TF7 4PG
0845 881 2222

Calls will cost 2p/min plus your telephone company’s access charge.

Request Catalogues & Brochures

Order the latest information on products and technology to be sent directly to you.

Catalogue  Brochure Request
Order Now

Surge protection technology

Find out about the basics, applications, and standards.

Surge protection technology
Find out more

1.5 billion contacts like this

Push-in connection technology – only from Phoenix Contact.

Push-in connection technology
More information

Find a distributor

Find out more about Phoenix Contact's distribution partners in the UK

Find a distributor
Find a distributor

This website uses cookies, by continuing to browse, you agree to our cookie policy. Read our privacy policy for more information.

Close