News Overview

New version of the UPS-CONF UPS software

13.08.2015

UPS-CONF configuration and management software, UPS systems QUINT UPS-IQ and TRIO UPS  

UPS-CONF enables UPS systems to be monitored and configured conveniently and clearly

The free UPS-CONF software enables the QUINT UPS-IQ and TRIO UPS UPS systems to be monitored and configured conveniently and clearly. The new version 2.2.7.0 features improvements and enhancements.

New warning messages signal, for example, whether the UPS remote control is activated or whether a communication error has occurred between the UPS and the batteries. The new COM trigger mode can be useful if several PCs need to be shut down in a controlled manner in the event of a mains failure; here the signal contacts of the UPS initiate a shutdown of the PC via the COM port, which means that no permanent data cable connections are required, regardless of the Windows version being used. DC UPS devices with 5, 10, 20, and 40 A from revision 06 can now switch off loads in a staggered sequence. When the UPS buffers a mains failure, two separate timers start, whereby previously defined consumers cease to be supplied by the battery after a set time. The software automatically detects the connected power storage, for example a lead battery with 12 Ah. All relevant operating parameters are displayed graphically and important messages appear in the foreground. The behavior of the UPS modules can be changed via the software to suit individual requirements.


PHOENIX CONTACT Ltd

Halesfield 13
Telford
Shropshire
TF7 4PG
0845 881 2222

Calls will cost 2p/min plus your telephone company’s access charge.

This website uses cookies, by continuing to browse, you agree to our cookie policy. Read our privacy policy for more information.

Close