News Overview

Surge protection for LED lights

06.04.2015

Surge protection for LED applications  

Surge protection for LED applications

The new surge protective devices for LED applications prevent the destruction of sensitive ballasts caused by overload.

They can be installed both in the connection box in pylons, as well as directly in front of the ballast of a lamp. As there is increased insulation, they can be used in LED applications in protection class II equipment. For grounded systems there is a protective device available with PE connection. The state of the protective devices is indicated directly on the device itself. The L connection can be used to transfer the signal to the lamp. If the surge protection disconnect device has been triggered due to overload, then the light is also switched off. This makes servicing and routine inspection of the surge protective devices significantly easier.


PHOENIX CONTACT Ltd

Halesfield 13
Telford
Shropshire
TF7 4PG
0845 881 2222

Calls will cost 2p/min plus your telephone company’s access charge.

This website uses cookies, by continuing to browse, you agree to our cookie policy. Read our privacy policy for more information.

Close