News Overview

Retrofit solution for detection and evaluation of lightning strikes

22.09.2015

LM-S control cabinet  

Turn-key solution for lightning measurement in wind turbines

If lightning damage on wind turbines (WTGs) remains undetected, this can have far-reaching consequences, particularly in the case of offshore parks.

To avoid expensive downtimes even in existing systems, Phoenix Contact has developed a retrofit solution for continual detection and evaluation of corresponding events. The core element of the solution is the lightning monitoring system (LM-S). It measures the strength and power of strikes and forwards them to operators in order to coordinate maintenance work. In the control cabinets for pitch control, there is very little room for subsequent mounting of the corresponding evaluation unit. The LM-S is therefore housed in a separate, space-saving control cabinet, that can be easily integrated into the automation landscape. The evaluation unit is supplied with power via its own power supply, from the QUINT product range. An uninterruptible version from the series can be installed, if desired. In order for the retrofit system to continue working without errors, even in the event of a lightning strike, all incoming and outgoing cables must be connected with surge protection.


PHOENIX CONTACT Ltd

Halesfield 13
Telford
Shropshire
TF7 4PG
0845 881 2222

Calls will cost 2p/min plus your telephone company’s access charge.

This website uses cookies, by continuing to browse, you agree to our cookie policy. Read our privacy policy for more information.

Close