References

References for control cabinet manufacturing

Expert partner

Your partner in control cabinet manufacturing.

The references listed here illustrate the wide range of possible solutions featuring COMPLETE line that have been implemented by well-known companies. Phoenix Contact is your expert and experienced partner for all your requirements in the field of control cabinet production.

Control cabinet production in the drinks industry: Cost-effective, even with a lot size of one

Control cabinet production at Krones AG

Optimization of control cabinet production at Krones, thanks to the ClipX concept

As a global manufacturer of bottling and packaging systems, Krones AG continuously strives to optimize not only its solutions, but also its manufacturing processes.

The concept from Phoenix Contact enables the ever-increasing number of control cabinets to be produced quickly, cost-effectively, and without errors in a lot size of one.

Automated terminal strip marking at W. Althaus AG: High efficiency and quality

Automatic marking at W. Althaus AG  

Laser cell for the automatic marking of terminal blocks

As a full-service specialist for industrial automation, one of the services that W. Althaus AG provides is control cabinet manufacturing. Along with the company's own Athex terminal block assembly machine, a marking solution from Phoenix Contact has helped increase productivity.

The ClipX.TerminalMarking system is the first solution of its kind for efficient, fully automated marking. To this end, a selected range of terminal blocks from the company's own portfolio are already fitted with special marking material before assembly. The components can then be marked just before they are attached to the DIN rail.

Laser marking technology is used here. This combination of material and technology results in high-contrast and precise printing. Looking at the versatile range of applications, this solution is just as durable as other combinations of material and technology. A fully automated manufacturing process can therefore be implemented.

Safe rail transport: Reliable data transmission requires faultless contacts

Rail transport safety  

Voestalpine diagnostic systems ensure safe and smooth rail transport

In comparison with other means of transportation, the railway offers the greatest degree of safety. Voestalpine Signaling Siershahn GmbH specializes in operational safety and maintenance in rail transportation.

To enable the quick installation of safety systems in railway lines and the reliable transmission of data to evaluation systems, the company relies on Push-in direct connection technology from Phoenix Contact.

For all electrical structures through to ready-to-use systems, Voestalpine consistently uses pre-assembled conductors with ferrules. Conductors pretreated in this way can be wired easily and without tools in the Phoenix Contact Push-in connections thanks to the low insertion force of the nominal cross section down to a cross section of 0.34 mm².

Push-in terminal blocks save time and space in elevator manufacturing

Bespoke elevators  

OSMA manufactures bespoke elevators

Elevators today are more than just a means of transporting people or loads safely: they are also design features, the calling card of a business, and an eye-catching statement.

However, these aesthetic considerations by no means push the technical functions into the background. As there is increasingly less space available for the electrical engineering, elevator manufacturer OSMA relies on compact Push-in terminal blocks from Phoenix Contact.

System cabling used on one of the world's longest suspension bridges

The Osman Gazi Bridge in Istanbul  

The Osman Gazi Bridge, one of the world's longest suspension bridges

Located approximately 50 kilometers southeast of Istanbul, the Osman Gazi Bridge, one of the world's longest suspension bridges, was built in the Gulf of Izmit.

System cabling and plug-in Push-in double-level terminal blocks from Phoenix Contact ensure that the countless I/O modules of the controller are connected to the field wiring quickly and without any errors. The significant reduction in installation time was crucial in meeting the tight construction schedule.