News Overview

Phoenix Contact’s newly expanded range of fuse and disconnect terminal blocks for explosive areas

23.09.2014

Phoenix Contact has expanded its range of fuse and disconnects terminal blocks with screw connection to include a new variant for use in potentially explosive areas (Zone 2).

The new terminals meet the requirements of the following ignition protection concepts:
CSA
• Ex nA IIC Gc
• AEx nA IIC Gc
• Class I zone 2
• Class I, Div. 2, Groups A, B, C, D

IECEx
• Ex nA IIC Gc


ATEX
• X II 3 G Ex nA IIC Gc
• Ex i

The new Class1Div2 fuse block is a plug-in element rated up to 6.3A in explosive area.
The new separation and isolating blade terminals are characterized by their compact design and high current-carrying capacity of up to 20A.
The double bridge shaft allows individual potential distribution and supply.


PHOENIX CONTACT Ltd

8240 Parkhill Drive
Milton, Ontario L9T 5V7
1-800-890-2820

This website uses cookies, by continuing to browse, you agree to our cookie policy. Read our privacy policy for more information.

Close