News Overview

Network Manager with topology representation

23.04.2019

Packaging for the Network Manager software  

The Network Manager – easy startup and configuration

With the FL Network Manager software, Phoenix Contact network components can be started up, monitored, and updated easily.

In the new Version 3.0, the software has now been extended to include topology representation and the SNMP scripting function.

To ensure the reliable operation of your networks, your network components not only need to be configured correctly, but also accurately connected to one another. The new topology representation enables you to check and visualize the device connections for each network port. This means that you can determine whether the actual network structure corresponds to your planned structure. In addition, topology representation also allows you to check the configuration of the redundancy protocols. Thanks to the use of different colors, you can see important information at a glance, such as the roles of the individual ports and devices in the redundancy system and the resulting redundant paths.

SNMP scripting enables you to easily perform more in-depth diagnostics on the network structure, e.g., in the event of an error. Version 3.0 of the Network Manager allows you to read the SNMP parameters of any device in the network, providing you with a current overview at all times.

Interested? You can download a demo version from our homepage free of charge to try the software for yourself.


PHOENIX CONTACT Ltd

8240 Parkhill Drive
Milton, Ontario L9T 5V7
1-800-890-2820

More Information

This website uses cookies, by continuing to browse, you agree to our cookie policy. Read our privacy policy for more information.

Close