News Overview

Safety in the cloud

28.11.2017

Cloud-based safety solution  

Cloud-based safety solution

Phoenix Contact will be presenting a cloud application for recording and analyzing safety-related data for the first time at the SPS IPC Drives 2017 trade fair.

With the PROFICLOUD solution, companies receive important information on the optimization of sequences in production. The safety of machinery is and remains a critical subject for machine operators, plant engineers, and systems manufacturers. Their first priority is the safety of machine users, but this can also cause unplanned operational interruptions. A common cause of failures is inadequate design. The ability to access safety system data via the Internet of Things (IoT) in real time and to convert this into meaningful information unlocks enormous potential. With Phoenix Contact cloud-based solutions, status information on standard- and safety functions are transmitted continuously via a PROFINET control solution to the PROFICLOUD. This information is then evaluated there. Thanks to the holistic consideration of resources and machinery, completely new opportunities are opened up for operators and designers to increase the operational performance. This enables, for example, the determination of interdependencies between safety- and process parameters. Or the monitoring of operational and maintenance processes across the entire line during normal operation. With access to this information, measures can then be derived and operational patterns determined. The machinery design can thus be optimized and work sequences designed to be more efficient.