News Overview

Phoenix Contact E-Mobility successfully certified in accordance with IATF 16949

01.02.2018

Lady standing at a charging station, charging an electric vehicle  

We are reliable partners with the automotive industry, and offer innovative products for the electric vehicle charging process

Within the Phoenix Contact Group, Phoenix Contact E-Mobility GmbH is the center of expertise for electromobility components and solutions.

Our portfolio includes charging systems and charging controllers for DC and AC charging of electric vehicles. Combined with the right software, we can also implement your customized and high-performance charging infrastructure.

For the vehicle-side charging process interface, we offer what are known as vehicle inlets, which are built directly into the vehicle. Collaborating with automobile manufacturers brings with it particularly stringent demands in regard to work processes, product quality, and organizational structure. Certification in accordance with IATF 16949:2016 was established within the automotive industry to ensure these requirements are being met uniformly and internationally. Quality management system certification in accordance with ISO 9001:2015 is also a substantial component of this standard. We recently successfully acquired certification in accordance with both of these standards, so that we now meet the stringent requirements of the automotive industry.

You can download the corresponding documents in the right-hand column.