News Overview

DC/AC inverter for the DIN rail

25.08.2020

QUINT DC/AC inverter for the DIN rail  

QUINT DC/AC inverter for the DIN rail

With the new DC/AC inverter in the QUINT POWER family, Phoenix Contact offers a compact solution to generate alternating current in DC applications for the first time.

Use the DC/AC inverter for the DIN rail to convert direct current into alternating current and get a pure sine curve at the output. The manual selection of the AC output voltage via a signal terminal enables worldwide use. An integrated USB interface can be used to connect industrial PCs, for example. Furthermore, you can switch the inverter in parallel. By connecting two devices in parallel, you can increase the operational safety of your systems in the event of power supply failure or benefit from higher power. Switch three devices in parallel to create a three-phase grid. The three devices communicate with each other in real time, thereby synchronizing the 120° phase shift. This means that AC drives can also be operated. Due to the comprehensive signaling options and the wide temperature range from -25°C to +60°C, you can use the inverter flexibly.


PHOENIX CONTACT Ltd

8240 Parkhill Drive
Milton, Ontario L9T 5V7
1-800-890-2820