News Overview

Maintenance-free tower lighting in wind turbine generators

17.05.2016

Switchgear and controlgear assembly for tower lighting  

Complete system for tower lighting in wind turbine generators

In order to ensure the safety of employees in wind turbine generators, the towers must be illuminated safely.

To this end, Phoenix Contact offers a tower lighting system using maintenance-free LED lights. The LED lights are supplied centrally by an uninterruptible power supply (UPS) installed in the tower base. Even before climbing the tower, the service technician can find out the state of the UPS and the batteries. The powerful LED modules conform to the relevant standard EN 50308. They provide good luminous intensity even at low temperatures. Thanks to a service life of 50,000 hours, the lights do not generally have to be replaced. Due to the low current consumption of the LED technology, the lights also function as emergency lighting. In the event of power failure, the lights continue to be supplied via a central battery. The luminosity is then maintained at 50%. There is therefore enough light still available in the wind turbine generator for the service technician to safely descend.


PHOENIX CONTACT PTY Ltd

Unit 7, 2-8 South Street
Rydalmere NSW 2116

Fax: 1300 723 399
Customer Service Hotline
1300 786 411

More Information

This website uses cookies, by continuing to browse, you agree to our cookie policy. Read our privacy policy for more information.

Close