News Overview

New generation of TP 5000 touch panels

14.12.2015

TP 5000 touch panels  

Touch panels with high-performance PC platform

The TP 5000 series touch panels are being converted to a new hardware platform.

The change has become necessary because the current hardware platform has been discontinued. With a smooth transition in mind, we have converted to the recess-compatible hardware of the Basicline panel PC. There are still three different display sizes: 12.1 inch (30.73 cm), 15 inch (38.1 cm), and 17 inch (43.2 cm) available.


PHOENIX CONTACT PTY Ltd

Unit 7, 2-8 South Street
Rydalmere NSW 2116

Fax: 1300 723 399
Customer Service Hotline
1300 786 411

This website uses cookies, by continuing to browse, you agree to our cookie policy. Read our privacy policy for more information.

Close