SPS IPC Drives 2018

SPS IPC Drives 2018

Visit Phoenix Contact at Europe's leading specialist trade fair for electrical automation.

November 27-29, 2018 in Nuremberg
Hall 9, Booth 310

Welcome to Phoenix Contact at the SPS IPC Drives 2018 – we are looking forward to your visit in Hall 9, Booth 310.

Be “there” when we present our new PLCnext Store for control apps. Experience the boundless options of our open ecosystem. Implement your automation projects even faster or become a provider of apps. Discuss with us the change in automation – about new liberties through cloud systems and open control platforms. New business and income models are waiting for you - rethink automation!

We look forward to your visit. Phoenix Contact sends you cordial greetings – your key partner with creative solutions in network technology, electronics, and automation technology for your path to a smart world.

To make it easy for you to find our booth at the trade fair, we have provided the floor plan for SPS IPC Drives 2018 here.

Description
SPS IPC Drives floor plan [PDF, 70 KB]

Be our guest at SPS IPC Drives

Reserve a free ticket for your visit to the trade fair. To do so, click on the button below and register using the online registration number 1810371873.

Our product highlights at SPS IPC Drives

Phoenix Contact offers a comprehensive portfolio of products and solutions in the field of automation and digitalization that are impressive in regards to both quality and security in the age of the Internet of Things (IoT). We would like to introduce you to a selection of these in the following to give you a preview.

Experience the All-in-One solution for industrial identification with the new BLUEMARK ID generation. Using environmentally friendly UV LED technology, these devices process over 1350 different marking materials. BLUEMARK ID COLOR provides marking in color for the first time as well. Operating the printer is intuitive, thanks to its touch display. The clear menu structure offers lots of additional support, from how-to videos to automatic material recognition.

The PROJECT complete planning and marking software gives you complete support when designing your control cabinet. Import your electrical plans with a click of the mouse via interfaces to all popular CAE programs. The software automates many of the steps involved in designing your terminal strip and creating suitable marking. Then order your fully assembled product directly on line. In this way, PROJECT complete becomes your digital interface in control cabinet manufacturing.

Re-discover motor starter technology with safety. The new CONTACTRON pro version offers easy safety integration with safety evaluation and group shutdown in accordance with PL e, and is modularly expandable.

The new PTFIX system for individual potential distribution consists of ready-to-connect blocks in eleven color options, varying numbers of positions and mounting types, along with cross sections from 1.5 to 4 mm² in Push-in technology. These blocks with up to 18 contact points can be combined as needed and mounted on DIN rails or direct-mounted or installed with adhesive. Using the online configurator, you can meet all your needs – and do so with pricing information and rapid order options.

The trend toward miniaturization is continuing without interruption in the field of network cabling as well. The new compact M8 connectors supply the smallest devices with Ethernet and PROFINET, and offer up to 30% in space savings compared to M12 connectors. The symmetrically arranged contacts provide secure data transmission. Field devices are supplied with power simultaneously via Power over Ethernet.

The number of cable connections is increasing due to the ever increasing networking of intelligent manufacturing systems. Modular industrial connectors are the solution in this case. With HEAVYCON modular, you can flexibly combine contact inserts for power, signals, data, and compressed air in one housing. The new online configurator provides you with ideal support for designing and ordering your tailor-made connector.

Standards DIN VDE 0100-443 and DIN VDE 0100-534 specify when surge protection is required in low-voltage systems and where and how it must be installed. A revised edition of both standards has been in effect since October 1, 2016. The transition period for manufacturing already initiated plans and implementation ends on December 14, 2018. Come by our booth to learn more about the mandatory options for protecting buildings along with other useful options.

Ideally suited for simple, space-saving potential distribution: The PTCB single-channel electronic circuit breaker can be bridged to the CLIPLINE complete terminal block system. It offers a setting range from 1 to 8 ampere with a very small overall width. We will be introducing other product versions just in time for the SPS. Come by our booth and learn more about the universal device circuit breaker with a 6 mm overall width.

Protect your power supply system with just the right electronic circuit breakers. You can easily find just the right product for your application in our portfolio. Take advantage of the easiest handling during startup as well.

With the Fine Pitch series board-to-board connectors, Phoenix Contact is providing shielded and unshielded solutions for signal and data transmission for the first time. This range enables you to realize individual PCB orientations with different designs, stack heights, and numbers of positions in the compact 0.8 and 1.27 mm pitches.

M17-M40 PRO series circular connectors offer uniform solutions for signal and power transmission. Thanks to the unique ONECLICK fast locking system, you can connect your device quickly and safely. The non manufacturer-specific connection compatibility enables you to realize versatile solutions for standard and fast locking systems.

Modular ICS series electronics housings form the basis for tomorrow's IoT devices: Take advantage of the unique modularity in the connection technology, with standardized connections such as RJ45, USB, D-SUB, and antenna sockets as integrated components. Furthermore, you can also benefit from a housing system with graduated sizes and optional DIN rail connectors.

Our tips for your visit to SPS IPC Drives

You will find our personal tips for your visit based on two decades of trade fair experience here.

The Nuremberg Exhibition Center can be reached easily and quickly by car, train, plane, or public transportation. U-Bahn (subway/underground) lines U1 and U11 (toward Langwasser Süd) will take you directly from the main railway station to the Exhibition Center. The journey time from the main railway station to the trade fair is only eight minutes.

Just enter Nuremberg into your navigation system. One of the most modern traffic and parking direction systems in Europe will guide you to your destination. Dynamically adjusted to the current traffic situation, it will direct you along uncongested approaches and to one of around 14,000 parking spaces around the Exhibition Center.

Demand for hotels near the Exhibition Center is high during SPS IPC Drives. If you are looking for something a bit farther away, the city of Nuremberg and its immediate surroundings offer perfect accommodation opportunities. It is worth a look: the surrounding communities also offer inns and interesting accommodation options where you can relax after an exhausting day at the trade fair.

Trade fair information for SPS IPC Drives 2018

We look forward to seeing you. Visit Phoenix Contact in 2018 at Europe's leading specialist trade fair for electrical automation in Nuremberg:

  • November 27 - 29, 2018
  • Hall 9, Booth 310
AddressOpening times
NürnbergMesse
Messezentrum 1
90471 Nürnberg
Tuesday from 9:00 a.m. to 6:00 p.m.
Wednesday from 9:00 a.m. to 6:00 p.m.
Thursday from 9:00 a.m. to 5:00 p.m.

For more information on the trade fair city of Nuremberg, the trade fair program, exhibitors, accommodations, tickets, tours, and much more, visit the SPS IPC Drives website.

A look back at SPS IPC Drives 2017

Phoenix Contact exhibition booth 2017  

Phoenix Contact exhibiting at SPS 2017

Phoenix Contact is pleased to report that the 2017 trade fair was a success.

The SPS IPC Drives 2017 recorded 70,264 visitors and 1,675 exhibitors on a trade fair area of 130,000 m².

Visitors showed particular interest in future-oriented themes of digital automation. Based on it, exhibitors and visitors addressed questions like where are we headed, what awaits us, how should applications be designed today for tomorrow.

Phoenix Contact has already demonstrated some answers with innovative products and solutions: we are blazing the trail toward digitalized industry with our industrial communications solutions, electronic circuit breakers, stable WLAN for machine building, new technology for an open control platform, and industrial cloud solutions.

What is SPS IPC Drives?

SPS IPC Drives is Europe's leading specialist trade fair for electrical automation. You will find the perfect platform for your search for the right solutions for your automation tasks in Nuremberg. Among other things, products and services from the following areas are presented:

  • Control technology
  • IPCs
  • Electrical drive technology
  • Operation and monitoring
  • Industrial communication
  • Software & IT in manufacturing
  • Interface technology
  • Mechanical infrastructure
  • Sensors

Come and see us for an overview: we will help you find the topics to match your specialization. Feel free to contact us for more information; we will be happy to help you at our booth in Hall 9.

Phoenix Contact at SPS IPC Drives

Phoenix Contact exhibition booth 1993  

Phoenix Contact at SPS IPC Drives 1993

Phoenix Contact participated in this trade fair for the first time in 1993. At that time, there were a total of 156 exhibitors and 4,923 visitors. Up until 1996, SPS IPC Drives was held in Sindelfingen, after which it moved to Nuremberg in 1997.

For the past 25 years, Phoenix Contact has been present at the trade fair in Nuremberg every year to showcase its innovations in automation technology. The title of the first of these trade fairs in which Phoenix Contact participated -back in 1993 - was: International Specialist Trade Fair and Conference for Programmable Logic Controllers, Industrial PCs, and Electric Drive Technology.
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
Our booth

Download a map of our both and use it for your visit at the fair.

Our booth
Open map [PDF, 51 KB]

See more of the SPS IPC Drives on YouTube

Experience our highlights of the exhibtion.

See more of the SPS IPC Drives on YouTube
To the YouTube Channel

More Information