NACS – the charging standard that is conquering the American market The North American Charging Standard, also known as the NACS and SAE J3400 standard, will play a central role in the electrification of the transport sector. The NACS standard will support and shape the development of the charging infrastructure for electric vehicles in North America.

Person charging a car in the garage

2024-12-15

Joe S. Boyer, E-Mobility Product Marketing Specialist, Phoenix Contact USA

Joe S. Boyer, E-Mobility Product Marketing Specialist, Phoenix Contact USA

In an interview with Joe S. Boyer, E-Mobility Product Marketing Specialist, Phoenix Contact USA, he explains how NACS will revolutionize the charging infrastructure in the USA in the coming years. Boyer is responsible for the technical support of internal sales staff and for the technical training of Phoenix Contact’s internal service teams in North America.

NACS charging connectors from Phoenix Contact

NACS charging connectors from Phoenix Contact

The key to the e-mobility revolution in North America is NACS

*“NACS became very popular when it was opened up for use by others besides Tesla,” explains Joe S. Boyer. “The NACS charging system developed by Tesla for electric vehicles in Canada, the USA, and Mexico is supported by a reliable and robust charging infrastructure network. The rapid market penetration has prompted many players in the North American e-mobility market to adopt NACS for their own products. The Tesla standard was opened up to other manufacturers in 2023 and was quickly adopted by many of them for their upcoming electric cars. In the meantime, almost all electric car manufacturers are planning to use it in the future,” reports Joe S. Boyer. “By opening up the standard, other manufacturers besides Tesla can produce NACS charging cables and NACS vehicle charging interfaces, including Phoenix Contact. In 2025 and 2026, the first non-Tesla electric cars for the North American market will roll off the production line with an NACS charging interface. With the new players in the NACS sector, we can expect many more developments in the market – including the expansion of the NACS charging infrastructure,” says Joe S. Boyer.

Type 1 standard HPC charging connector

Type 1 standard HPC charging connector

What impact will this have on the type 1 charging standard in North America?

“The North American Charging Standard (NACS) is gaining momentum and will replace the CCS type 1 charging standard in the long term. However, the J1772 (AC) and CCS type 1 (DC) charging standards will not disappear from the market immediately. They will remain in place for at least the next 6 to 8 years and then gradually become less important as the number of NACS vehicles increases,” says Joe S. Boyer. “There are a large number of electric vehicles that still have CCS type 1 vehicle charging inlets, so we have to continue to support them with charging infrastructure. The nature of the market for utility vehicles also indicates that the CCS type 1 standard will remain in place for the time being. In the long term, however, the new NACS standard will also prevail here,” reports Boyer.

Is it possible to easily switch from type 1 to NACS?

*“Whether electric vehicles with an existing type 1 interface can be converted to an NACS charging interface depends on whether or not they are designed with the same basic profile for the connection. From the point of view of the hardware, the installation dimensions can be the same as for type 1, but the cabling would have to be drastically changed,” explains Joe S. Boyer. “The software must also take all these changes into consideration, as the same pins are used for AC charging and DC charging in the NACS charging inlet. All in all, retrofitting the charging interface in the vehicle is too expensive and is therefore not recommended. The simpler solution for EV owners is to use an NACS-to-CCS1 adapter and/or to use charging stations that offer both a CCS1 and an NACS charging connector.”

CCS1 charging station, USA

CCS1 charging station, USA

And what about the charging stations?

“The changes to the charging stations are not as significant as those on the vehicle side. NACS and the J1772/CCS1 standard have the same necessary contacts for charging, so the cables can be easily swapped if necessary. Depending on the design of the charging station, minor changes may have to be made inside in order to establish the new connection. Not much is needed to physically update a charging station. Thanks to the standardized communication methods in the industry, communication with the vehicle will be no different.”

US flag

How is the market in North America developing with regard to the new NACS charging standard?

“The focus is currently on preparations for 2025 and 2026. Companies are evaluating future options and working with test samples, but overall, the NACS rollout will take some time. The requirements for the connectors vary depending on the application, but are essentially comparable with the type 1 standard. Charging power expectations are based on the standards used in North America, with development aimed at making charging faster and more efficient over time. Charging connectors and vehicle charging inlets must be designed to be reliable and have a long service life, reflecting the proven quality of Phoenix Contact.”

E-mobility charging park, USA

E-mobility charging park, USA

Are there specific policy objectives for the ramp-up of NACS charging infrastructure in the USA?

“Nothing is planned at the moment,” is how Joe S. Boyer summarizes the current situation. “The federally funded National Electric Vehicle Infrastructure (NEVI) program to expand charging infrastructure on all major highways currently requires the use of CCS type 1. The program would need to be amended for NACS to receive government-funded support. However, NACS is already supported by a robust charging infrastructure network, which means that it can stand on its own two feet.”

NACS charging cables from Phoenix Contact

NACS charging cables from Phoenix Contact

NACS products from Phoenix Contact:

NACS products from Phoenix Contact will hit the market offering proven industrial quality. First to be launched on the market in Q1/2025 are the 100% standard-compliant NACS AC charging cables in the CHARX connect eco family, which comply with the SAE J3400 North American automotive standard and offer maximum safety. The robust NACS charging connectors are easy to handle and enable AC charging with up to 80 A. Joe S. Boyer predicts: “In 2025, the first non-Tesla vehicles are expected to be tested and introduced to the North American market in small quantities. In the following year, further vehicles are expected on a large scale, which will benefit not only Tesla but also the manufacturers of charging infrastructure.”

Certified in accordance with UL 2251, the NACS AC charging cables from Phoenix Contact have passed all UL safety tests. For electrical safety, the power contacts of the NACS charging connector are equipped with touch protection that meets IP2XB degree of protection in accordance with UL requirements. Fully molded plastic caps on the protruding pins of the power contacts ensure that this is permanently the case. As Boyer explains: “This prevents electrical accidents caused by exposed power contacts and also increases the reliability of NACS charging stations.”

The optional integrated temperature sensors protect against overheating, while the complete longitudinal water tightness of the charging connector protects the live parts of the electrical system. These properties help to ensure a long service life for the NACS charging cable. In line with the installation requirements of NACS charging stations, AC charging connectors are available with a 25-foot-long, unassembled cable or can be individually assembled according to customer requirements. Customizations can include flexible stripping lengths and step-by-step cutting, crimping, or sealing using ultrasonic welding technology.

Charging park

Outlook for further NACS products from Phoenix Contact: DC charging cables and vehicle charging inlets

The Phoenix Contact development team is working day in, day out on innovative products for the North American charging standard.

NACS DC charging cables: DC charging cables for fast charging with 200 A and 375 A (uncooled) and 650 A (liquid-cooled) will be available from 2025. These charging cables are specially designed for high charging powers and enable fast and efficient charging.

Customer-specific NACS charging inlets: Customer-specific charging inlets for automobile manufacturers will be developed in parallel. These will be customized to the needs and specifications of the respective manufacturers in order to ensure optimum integration into the vehicles.

Universal NACS vehicle charging inlets: Available in various performance classes from 2026 for utility vehicles, mobile machinery, and the transport sector. These vehicle charging inlets are versatile and offer a flexible solution for various applications in the transport and utility vehicle sector.

Further information on NACS products from Phoenix Contact is available here:

Author: Katharina Strunk


Your personal contact person

For all queries regarding our products and solutions

Michael Brooks
Michael Brooks
Market Segment Manager – E-Mobility
+1 810 513-6042
I would be happy to advise you on your e-mobility project. Let’s shape the mobility transition together!