Large-volume outdoor housings for the reliable operation of autonomous device systems

2023-02-27
OCS outdoor housings for autonomous systems

The OCS series outdoor housings from Phoenix Contact provide excellent protection for autonomous device systems.

Even in extreme environments, the large-volume housings reliably protect the electrical components inside. Valuable electronics are thus permanently and reliably protected against humidity, heat, UV radiation, and mechanical strain. Even jet water does not penetrate. The certified polycarbonate housings are lightweight and resistant. They even withstand heavy mechanical strain within a wide temperature range. The housing system is approved for numerous electronic systems by international approvals. The solutions in the OCS series offer a high degree of flexibility and can be individually adapted and extended with accessories.

Press Contact
Eva von der Weppen
Eva von der Weppen | Corporate Communications