Individual service for signal integrity
The demands on connection technology performance are constantly increasing. By providing customized support, Phoenix Contact helps customers select connection components to ensure the highest possible signal integrity. This is based on experience in the development of standardized data connectors for various device interfaces.
Phoenix Contact provides customer-specific design-in support for device-internal connections, which are usually not fully standardized. Simulations are used as the basis for advice on the selection of suitable connector combinations and contact assignments. This requires just a few details about the respective application, such as the arrangement of the printed circuit boards in the device, the type of data transmission, and the target impedance of the system. The individual simulations can usually be realized within a few days and are documented comprehensively.