High flexibility and a narrow design

2022-05-19
VARIOFACE Front Connect

The new generation of highly compact VARIOFACE Front Connect termination boards from Phoenix Contact supplements the cabling area between the remote I/O system and the field level.

The user-friendly design ensures fast and error-free wiring as well as space savings in the control cabinet. The termination board supports the decentral I/Os with high flexibility and a narrow design.

The controller-specific system cabling was specially developed to allow quick, error-free connection to the I/O modules of a wide range of controllers. The new generation’s easy-to-plug front adapters, system cables, and termination boards save up to 90 percent of the time needed and 60 percent of the space compared to conventional solutions.

Press Contact
Eva von der Weppen | Corporate Communications