Employee uses cloud computing technology on a tablet

Cloud computing The future of the industry

Back in 2017, the famous quote “The world’s most valuable resource is no longer oil, but data” came about. In 2021, this is even more true. In every industry, large amounts of data are generated every day, but in many cases this data has hardly been used yet. Proficloud.io makes this data usable. Proficloud.io gives small and medium-sized enterprises the opportunity to participate in the digitalization of their industries, to harness the data that accumulates, and thereby to optimize their own processes, save costs, and increase their speed.

Diagram explaining cloud computing with connections of the various interfaces via the cloud

What is cloud computing?

In the past, anyone who wanted to use computing capacity was forced to operate their own servers. The required resources had to be calculated and procured, updates had to be installed, backups had to be set up, and the availability of the servers had to be ensured. As a result, companies either expended huge amounts of resources (human and financial) or had to accept cutbacks.

Thanks to the cloud, that’s a thing of the past. The server previously located in the company is now being replaced by professionally operated data centers – the cloud. Resources such as computing power or memory capacity can be provided in virtually unlimited amounts at any time. This works so quickly that even peak loads can be balanced. Issues such as software updates or creating backups are handled by the operator of the respective cloud platform. The cloud opens the door for companies to participate in the world of data – without great cost or effort.

Diagram explaining cloud computing technology

What is the technology behind it?

In the area of technologies used, MQTT is certainly worth mentioning. MQTT is a protocol that is primarily used for communication between machines. In our case, this is the communication between the cloud-capable devices in the field and Proficloud.io, which is handled via MQTT. For this purpose, MQTT offers several advantages at once, such as low computing power requirements, low overhead, and secure communication through TLS encryption.

Icon illustrating the features of cloud computing with cloud and tablet

Features

There are different varieties of cloud systems, but the following points apply to many of them:

  • The existing hardware is shared among different users. This makes it possible to keep costs low, yet still keep the data separate.
  • The required performance can be scaled up or down at short notice. This makes it possible to react quickly to changes.
  • Cloud services are not purchased, but rented. Since every cloud system requires continuous effort from the operator, this is the only way to map the costs involved. This offers the customer the advantage of not having high start-up costs (CAPEX), but instead being able to stretch predictable costs over a longer period of time (OPEX).
  • Since the expenses for operating and maintaining the cloud are covered by the operator, use is low-cost for customers. The customers can focus directly on their actual interests.
Icon to illustrate the risks in cloud computing

Risks

Cloud computing with Proficloud.io:

  • Our user's data is stored in a data center in Frankfurt, Germany.
  • We are GDPR-compliant.
  • The transmission of data between the devices, customers, and Proficloud.io is always TLS-encrypted.
  • Data is not be shared with other parties under any circumstances. We view our customers’ data as just that: our customers’ data, not our data.

Proficloud.io and Smart Services

Ultimately, this question remains: How can your company also benefit from the advantages of the cloud? In other words, how do you start using Proficloud.io? Proficloud.io consists of a series of Smart Services that serve different use cases and therefore also fit many different kinds of companies.
You can find an overview of these Smart Services here: